Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the RSTP roles in Easergy P3
RSTP role of the port. There are four possible roles:
- Root (by this port, the device communicates with the RSTP root, directly or by other devices. This port is a part of the shortest path to the root)
- Designated (through this port, network traffic is passed to the subnetwork. There should be only one RSTP port marked as designed for each subnetwork/segment)
- Backup (this is the backup/redundant port connected to subnetwork/segment. If the designated port loses connection, this port can become designated)
- Alternate (this is the backup/redundant connection to the root. If the root port loses connection, this port can become root)

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings