Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there any recommendation of communication cable (Example Modbus) for ATV71 drives.
Regarding communication cable (for example Modbus); following are the recommendation: ----
-Use the cable with 2 pairs of shielded twisted conductors.
-Keep the communication cable away from the power cables (30 cm minimum).
-If it is necessary for the Modbus cable and the power cables to cross each other, be sure they cross at right angles.
-Whenever possible, connect the cable shielding to the protective ground, e.g., to the ground of each device if this ground is connected to the protective ground.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings