Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the inspection and check points for ATV630 drives.
Visual Inspection:-
During visual inspection the overall condition of the inverter installation should be checked for following points:
-Mechanical damages of the housing
-Traces of oxidation caused by humidity, aggressive gases, or liquids
-Dust sedimentation inside the inverter, especially conductive dust
-Dirt and dust sedimentation on the heat sink and the motor terminal board
-Damages of cable isolation (especially at the inverter lead-through)
-Traces of humidity and water inside the cubicle

Checks:
-Perform the following checks:
-Take the actual parameter settings and compare them with the commissioning settings
-Check of the electrical plug connections (connection correct and fixed) and check connector pins for oxidations
-Check the conditions of the enclosure gaskets
-Check the diagnostic LEDs,

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings