Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is LRF fault on ATS48.
LRF fault is Locked Rotor in continuous operation Fault .
The locked rotor fault is checked in continuous operation, ATS bypassed Fault threshold: motor current measured > 5*In for 200 ms in one phase This fault is stored in the EEPROM fault log.
=>Increase (if possible) the value of the In parameter (nominal motor current).
=> Check that the rating of the ATS and the motor are sufficient for the application.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings