Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is THSC(E21) fault on Altivar AFE.
Monitoring of the internal temperature sensor (short-circuit at a thermistor sensor).
A thermistor of the heat sink is short circuited (value <50 Ω).
Remedy: Check the display in parameter 1.1.08. If it is 0 % or higher than 118 %, probably a temperature sensor is defect. It can be only exchanged by authorized service
technicians.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings