Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why no relevant information is available in Syslog.dat log file
Log information is stored in Syslog.dat when the Citect runs as a single process, but log files may have additional suffixes included in their name when running in multi-process environment, for example, an archived log file will include a timestamp (see Log File Time Stamping).

If a system uses separate processes(multi-process), a log file is appended with the component name. An example of this could be:

syslog.IOServer.Cluster1.dat

Citect SCADA log files are stored in the Windows Program Data directory, by default.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings