Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Getting Error 1800: [Target] [target name] cannot find defined target machine, while downloading program in the HMI

When downloading, connection with the target machine could not be established.

Solution:

When using Serial or USB download, the error message appears due to one of the following:

  • Target machine is OFF.

  • Download cable is not connected to the defined port on the editor PC.

  • Download cable connections are loose.

  • Invalid download cable is used.

  • Download cable is damaged.

  • Connected target machine is not supported.

When using Ethernet download, the error message appears due to one of the following:

  • Vijeo-Designer Runtime is not running or the target machine is not turned ON.

  • You entered an incorrect IP address in the Target's download properties.

  • The IP address set in the Target properties is not for a valid Vijeo-Designer target machine. You probably typed an IP address that belongs to other types of equipment.

  • You used Download All on a project that has more than one target set to the same IP address.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings