Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to copy a backup set to the Enterprise Server or Enterprise Central local directory.
Please refer the procedure as below:
  • In WorkStation, in the System Tree pane, select the Enterprise Server or Enterprise Central you want to configure.
  • Click the Control Panel tab.
  • Click Backup and Restore Manager .
  • In the Backup sets path box, copy the entire backup sets path of the Enterprise Server or Enterprise Central.
  • Open a browser, such as Windows Explorer.
  • In the browser Address box, paste the backup sets path and press Enter .
  • In the db_backup folder, open the LocalBackup folder.
  • Right click the backup set that you want to copy and click Copy .
  • Navigate to the db_backup folder of the Enterprise Server that you want to restore.
  • Paste the backup set into the LocalBackup folder of the targeted Enterprise Server.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings