Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
what is the reason for atv320 showing 'CONP' while entering JOG menu
It's not an error but a display which means incompatibility. It's due to the other function used in the drive which is incompatible with the 'Jog' function.

Refer the attached compatibility matrix page extracted from the ATV320 manual for functions compatible with 'Jog' function & other functions compatibility.

Schneider Electric India

Attachment(s)
ATV320 compatibility.pdf [190.19 KB]
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings