Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How Communications between M580 safety PAC and safety I/O modules installed in an RIO drop will be done.

Communications between the safety PAC and safety I/O modules installed in an RIO drop are made through an adapter module installed on the RIO drop, either:
a BMECRA31210 adapter, for an Ethernet rack, or
a BMXCRA31210 adapter, for an X Bus rack.

NOTE: A BMXCRA31200 adapter cannot be used to connect safety I/O modules to the M580 safety PAC.

Communications from the safety PAC and safety /O modules, both in the local main rack and in an RIO drop, are made via the black channel.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings