Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the benefit of enabling "Automatic blocking of service port on Standby CPU" in M580 HSBY CPU.
Enabling "Automatic blocking of service port on Standby CPU " Automatically blocks the service port to help avoid an unintentional loop.
NOTE: These features are implemented in a Hot Standby system using a CPU with firmware version 2.7 or later and a BMENOC0301.4 or later module and this check box is available only in Unity Pro 13.1 or later.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings