Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the minimum Firmware Requirement to support IP forwarding service with BMENOP0300 module.
The IP forwarding service is supported by the following versions:

BMENOP0300 firmware version ≥ V2.0
Modicon IEC 61850 Configuration Tool ≥ V3.0

NOTE: Only one of the following functions can be enabled at any time: the IPsec protocol, the Ethernet backplane port, or the IP Forwarding service.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings