Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the part reference of Output choke for ATV340
For the ATV340 there is no offer for motor choke.
Only DV/DT Filters are available

Note: ATV340U07...D22N4, ATV340U07...D37N4E drives are compatible to be used with maximum 100 m/328.08 ft shielded motor cable length with 4kHz switching frequency.
ATV340D37...D75N4E drives are compatible to be used with maximum 100 m/3.28.08 ft shielded motor cable length with 2.5kHz switching frequency

It is recommendable to use Shielded cable, as non-shielded cables can worsen the EMC behavior.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings