Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How we can make a switchover between redundant 140CRA31908 modules using application logic.
You can use system bit %S88 to reassign the master of the I/O points. When %S88 is set, the system triggers a 140CRA31908 switch over and assigns the role of I/O master to the other 140CRA31908. The system then resets %S88.

NOTE: In redundant 140CRA31908 module configurations, check the status of the redundant 140CRA31908 module before a switchover is triggered. If the redundant 140CRA31908 module is not healthy, the system does not allow the switchover (even if %S88 is set).

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings