Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to assign multiple 140CRA31908 as I/O master.
NO, Only one 140CRA31908 module is assigned the I/O master at any time. The master 140CRA31908 module can perform these tasks:
  • Manage I/O modules over the S908 network.
  • Manage I/O modules that are configured on its local rack.
  • Provide EtherNet/IP statistics.
  • Provide S908 network diagnostics.
In redundant systems, the 140CRA31908 module that is not the I/O master can perform these tasks:
  • Manage I/O modules that are configured on its local rack.
  • Provide EtherNet/IP statistics.
  • Monitor the S908 network.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings