Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between braking unit and network braking unit for ATV71 drive.
Braking Unit enables the Altivar 71 drive to operate while braking to a standstill or during "generator" operation, by dissipating the energy in the braking resistor.
ATV71HxxxM3, ATV 71HxxxM3X, ATV 71H075N4…HC16N4, ATV 71WxxxN4,
ATV71PxxxN4Z and ATV 71HU22Y…HC16Y drives have a built-in dynamic brake transistor.
For ATV 71HC20N4…HC50N4 and ATV 71HC20Y…HC63Y drives, a braking unit is optional.

The network braking unit can be used to restore the following to the line supply:
(1) The energy from the motor
(2) The energy from motors controlled by several drives connected on the same DC bus.
It is available for ATV 71xxxxN4 and ATV 71PxxxN4Z drives.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings