Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the B10/B10d value of Harmony XB4/XB5 series of Estop push button?
For a complete push-button (including contacts), it is necessary to consider the B10/B10d of the contacts
For the contact, you should consider the electrical endurance according to the current and voltage used
B10 (e-Stop) = 300000 cycles
B10 (contact) = 1000000 at nominal current AC15 (230V, 2A)
B10 (complete PB) = min{B10(operator), B10(contact)} = 300 000
For E-Stop, B10d = B10/0.2
B10d (E-Stop) = 1500000

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings