Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How configure the Display and Beeper on an InRow ACRD200 cooling system.
Issue:
How configure the Display and Audible options on an ACRD200 cooling unit

Product line:
ACRD200

Environment:
All Serial Numbers

Cause:
Install, Configuration

Resolution:



Press ESC until you get to the main screen (On/Standby)

Use the Up or Down arrows to find the heading Configure Display

Press ENTER and select Contrast

Now you will be prompted for a password

Use the default password of “apc”

If this does not work check with your Admin for the correct password

If password has been lost use the last eight digits of the serial number

Press Enter and set Contrast from 1-10. This changes the brightness of the screen.

Press Enter on Key Click and turn On or Off. This allows every key on the display to make noise when used.

Press Enter on Beeper Volume you can select Low, Medium, or High. This controls the level of the Beeper volume in turned on.

Press Enter on Beep On Alarms and select ether On or Off. This enables the unit display to beep if unit is in alarm.

Schneider Electric India

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings