Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to change the SmartX Server TCP/IP Settings and Ports in EBO.
Please follow below steps to change the SmartX server TCP/IP settings and ports

1. In Web Station, in the Settings menu, click Options.
2. Click Device configuration.
3. Click the Network tab.
4. In the DHCP box, select Enable to obtain TCP/IP configuration information from a DHCP server.
5. In the IP address box, type the IP address of the SmartX server.
6. In the Subnet mask box, type the address of the subnet that the SmartX server belongs to.
7. In the Default gateway box, type the address of the node that serves as an access point to another network.
8. In the DNS server box, type the address to the DNS server where the SmartX server address is listed.
9. In the Domain name box, type the IP domain name that the SmartX server belongs to.
10. In the Host name box, type the IP host name of the SmartX server.
11. In the HTTP port box, type the HTTP port.
12. In the HTTPS port box, type the HTTPS port.
13. Click Save.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings