Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the mandatory requirement of enabling "Automatic blocking of service port on standby CPU" for M580 CPU.
Below are the requirement to use "Automatic blocking of service port on standby CPU" for M580 CPU:
  • CPU with firmware version 2.7 (or later) or a BMENOC0301.4 (or later).
  • Control Expert v 14 or later
NOTE: Unity Pro is the former name of Control Expert for version 13.1 or earlier.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings