Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to enable/disable "Automatic blocking of service port on Standby" on M580 HSBY CPU.
To configure, select the ServicePort tab.
  • Select the Automatic blocking of service port on Standby CPU check box so that the service port of the standby CPU is automatically blocked.
  • Deselect the check box so that the service port is not automatically blocked.
The check box is deselected (unblocked) by default.
NOTE: These features are implemented in a Hot Standby system using a CPU with firmware version 2.7 or later and a BMENOC0301.4 or later module and Control Expert v14 or later.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings