Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many events are stored in diagnostics buffer (without archiving) in M580.
The number of messages displayed in the list is defined solely by the size of the available memory.
If the memory becomes insufficient:
the DIAG information flashes in the status bar,
the messages associated with faults that have disappeared and have been acknowledged (if they needed acknowledging) are deleted.

The Size of Diag / Diagnostic buffer is 4 KB.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings