Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the safety I/O modules available in a M580 Safety PAC System
The following four M580 safety I/O modules are certified for use in safety applications:
 BMXSAI0410 (Analog Input)
 BMXSDI1602 (Digital Input)
 BMXSDO0802 (Digital Output)
 BMXSRA0405 (Digital Relay Output)

Use the four safety I/O modules to connect the safety PAC to the sensors and actuators that are part of the safety loop. Each safety I/O module incorporates a dedicated safety processor. You can install these I/O modules in the local backplane or in RIO drops.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings