Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to do Modbus RTU protocol settings in REL52813 and REL52814 (VIO 12AC/AD).
The REL52813 / REL52814 (VIO 12AC/AD) module's address is set with DIP switches. The available address range is 1–247. If RS-485 interface is used and there are multiple REL52813 / REL52814 modules
(or other external I/O modules) connected to the same RS-485 bus, then each module has to have a unique address. The termination must be on in the last module of the RS-485 bus structure.
The baud rate is fixed to 9600 b/s, and the parity is Even.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings