How to do RTD input protocol settings in REL52813 and REL52814 (VIO 12AC/AD).
By setting the REL52813 / REL52814 (VIO 12AC/AD) module’s address to ‘0’ it is possible to send RTD measurements to the relay via RTD input protocol.
Note: When implementing the connection between REL52813 / REL52814 and Easergy P3 relay with RS-485 via RTD input protocol it needs to be taken
into consideration that no other modules can be connected to the RS-485 bus. mA outputs and inputs cannot be used via RTD input protocol.
Note: When implementing the connection between REL52813 / REL52814 and Easergy P3 relay with RS-485 via RTD input protocol it needs to be taken
into consideration that no other modules can be connected to the RS-485 bus. mA outputs and inputs cannot be used via RTD input protocol.
Released for: Schneider Electric India