Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is displayed in Easergy Pro when there is a power failure or connection loss to the RTD module , when using RTD Input protocol.
In case of power failure or connection loss to the RTD module, when using RTD input protocol:
• Each sensor channel displays a value of -250ºC
• Timeout counter increases in the Protocol menu*

* If the application uses Remote- or Extension-communication port, an
alarm can be generated using relay logic, for for example inverted
Remote.comm signal can be used to drive a LED.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings