Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How Torque is calculated in ATV320 and ATV630 Drive
On ATV320 or ATV630, this parameter will be estimated  based on motor current measured.

The torque of motor is not measured by the drive. It is calculated from the measurement of motor
current.
OTR = (Iq / Iqn) * (PhirdRef / Phirn)
Iq : Current torque provide by the command to drive motor
PhirdRef : Flux provide by the command to drive motor
Iqn : Nominal Current torque compute with the motor name plate
Phirn : Nominal flux of the motor

Note - All values are in percentage

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings