Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video : How to set up load assist on a Uniflair unit.
Issue:
How to set up load assist on a Uniflair unit.

Product line:
Uniflair Gen 1 and Chilled Water Units.

Environment:
Uniflair units with push button displays and all Uniflair Chilled Water Units.

Cause:
Install, Repair, Maintenance.

Resolution:
These are the instructions on how to set up a Uniflair unit to turn on for load assist. Load assist in a Uniflair united is referred to as Sleep Mode. We need to make the proper adjustments to make the unit come on as needed. This operation will only work with two or more units and they must be grouped together.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings