Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can EBO 2.0/3.0 objects (XML) be imported in SBO 1.x or EBO 3.0 objects in EBO 2.0.
Import and Export is supported for all newer major or minor versions but a higher version export cannot be imported to lower version.
If attempting to do this, you will see an error something like below:
ERROR: Import failed to complete with an exception: RecoverableException: d:\dev\rb-RB-1.9.3-system\source\server\nsp_servers\csc\impex\source\ImportDispatcher.cpp(147)
Lonworks Error: Version_Error (0xd0017) in module Impex(57). "Import is only supported of exports from 1.x-releases!"

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings