Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to set speed around reference in ATV320 from HMI local display
Basic parameters for speed around reference:-

Set Fr1 – LCC (HMI)
Set Full àCtl- à CHCF à SEP (Because control command is from terminal and frequency reference is from local HMI)
Set Full à Fun- à SrE à uSi à LIx
Set Full à Fun- à SrE à dSi à LIx
Set à Fun- à SrE à SrPà % (Reference Speed i.e Fr1)

Note - If Fr1 is set to 50 Hz and SrP is set to 50%, then the speed will only go up to 50% of 50, i.e. 25Hz.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings