Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can we use BMXNRP0200 or BMXNRP0201 fiber optic repeater modules with M580 Safety system.
Yes, we can use BMXNRP0200 or BMXNRP0201 fiber optic repeater modules with M580 Safety system to extend the physical link between the CPU and Copro in the local rack and the adapter in the RIO drop.
Fiber optic repeater modules enhance RIO network noise immunity and increase cabling distance while maintaining the full dynamic range of the network and the safety integrity level.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings