Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I take the backup of the security system configuration in Vijeo XL

You can back up your project's security system configuration by exporting it to a file. You can also import a configuration either from a file or from another runtime project.

To export the security system configuration:

  1. In the main Security System dialog, click Backup. The Import/Export dialog is displayed.
  2. Click Export to file. A standard Save As dialog is displayed.
  3. Specify a file name and location for the file, and then click OK.

The exported file is encrypted, using the main password configured in the Security System dialog.

Tip: You can also export the configuration during runtime by calling the ExportSeruritySystem function.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings