Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Kiss-free mechanism of GV4 MPCB.
Circuit breaker closing is possible only if the voltage exceeds 85 % of the rated voltage. If an under-voltage condition exists, operation of the closing mechanism of the circuit breaker will not permit the main contacts to touch, even momentarily. This is commonly called "Kiss Free".

Schneider Electric India
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
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings