How can we help you today?

What are the specifications of the STO inputs on an ATV630

Characteristics of ATV Process STO inputs
PLC compatibility:      comply with IEC/EN61131-2 logic type 1 and type 3, for voltage levels
Positive logic (Source):
- state 0 if  ≤ 5Vdc or STO not wired,
- state 1 if ≥ 11Vdc
Impedance:     ≥ 2.2kΩ
Maximum current:      10mA min at 19V input for external (Preventa) Relay
Response time:      10ms

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings