Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why BTUA, BTUC and BTPI parameters are there if ATV320 does not have Bluetooth

For ATV320B or ATV320C there is no embedded bluetooth and the 437 specification does not exist.

Inside the ATV320 you can see BTUA BTUC BTPI because ATV320 come from ATV32 software. The Bluetooth module in not inside anymore, but the firmware was not changed on this part. The parameters have no influence inside ATV320.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings