Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can i find specification for VW3M1C20XX cable for Fabrication at locally


The VW3M1C10R is designed for max. 3m..It`s a shielded cable with 50pin connector on drive side and other end is open.
For longer cables below are the specifications
Cable specifications are valid for signal cables :
Shield: Required, both ends grounded
Twisted Pair: Required
PELV: Required
Minimum conductor cross-section: 0.14 mm2 (AWG 24).
The cable length depends on the signal type.
Do not use signals without push-pull (open collector) in the case of cable lengths of more than 3 m.
For push-pull max. 10m
RS422 max 100m is ok (fulfills RS422 standards ).

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings