Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the Maximum current input at CL1 and CL2 on ATS48CXXQ

ATS 48 •••Q: Altistart control power supply 220V to 415V, the maximum current input at CL1 and CL2 on ATS48C48Q is given below.

From the formula P = VI, you can calculate the current by following formula;

I = P/V

In case you provide power supply voltage 380VAC at CL1 and CL2.

I = 80W/380V = 0.211 A

See attached image

Schneider Electric India

Attachment(s)
ATS48_Image.jpg [35.22 KB]
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings