Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to Update the eCommission Bluetooth Adapter Firmware.
  • Connect to the Adapter.
  • In the Bluetooth Device Management page, select Update Adapter Firmware . If this button is read-only, the Adapter contains the latest firmware.
  • On the eCommission Bluetooth Adapter, press and hold the push button for 9 seconds. The LED displays the DFU mode flashing sequence. The eCommission SmartX Controllers mobile application displays the firmware upgrade progress.
  • When the firmware upgrade is complete, select Done .
  • Remove the Adapter from the SmartX Sensor.
  • Plug the Adapter back into the SmartX Sensor.
  • In the eCommission application, in the Bluetooth Devices page, select the Adapter and select Connect .
When you successfully connect to the Adapter, the firmware upgrade is complete.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings