Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to change the PIN of the eCommission Bluetooth Adapter.
Refer the below procedure to change the PIN:
  • Connect to the Adapter. In the Bluetooth Device Management page, in the PIN field, type the new PIN and select Update.
IMPORTANT: You cannot reset the new PIN to the factory PIN 333666.
  • Your mobile device or Windows 10 laptop prompts you to unpair from the Adapter. Select Allow.
  • The eCommission application returns to the Bluetooth Devices page. On the Adapter, push the LED button to initiate pairing.
  • In the eCommission application select the Adapter and select Connect.
  • In the Bluetooth Device Management page, select Discover Device.
  • Your mobile device or Windows 10 laptop prompts you for the Adapter PIN. Enter the new PIN and select Allow.
  • Your mobile device or Windows 10 laptop indicates the pairing was successful. Select Close.
  • You have successfully changed the Adapter PIN and can connect to a controller.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings