Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to configure Windows Firewall for Connect Agent in EBO.
Windows Firewall are configured for Connect Agent to ensure that the system and crash information is available on Connect storage server.
Refer the below steps:
  • On the Windows toolbar, select Start and then click Control Panel.
  • Click System and Security and then click Check firewall status.
  • Click Advanced settings and then click Outbound Rules. Click New Rule.
  • Select Program and click Next.
  • Enter the SE.SBO.S2ConnectESAgent.exe program path. (For example, C:\Program Files (x86)\Schneider Electric EcoStruxure\Building Operation x.y\S2ConnectAgent\bin\SE.SBO.S2ConnectESAgent.exe). Click Next.
  • Select Allow the connection and click Next.
  • Select the profiles and click Next.
  • In the Name box, type the name for the rule and click Finish.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings