How is a direct-wired serial ClearScada Server connection configured.
SCADAServer connections are configured in the Server | Connections dialog. To configure a direct-wired serial connection:
Select Server | Connections.
Select Add.
Highlight Serial Port and select the OK button to accept the selection.
Highlight the connection that requires configuration and select the Properties button.
Modify each field as required. Some of the fields include
Access Path: the name that is used by the OPC clients to indicate the path of communication from the PC to the field devices. This name may be changed to something more specific than the default value 1, e.g. PCCOM1.
Serial Port: pull-down list contains the names of all available computer COM ports, as detected by SCADAServer.
Addressing: pull-down list contains the selection of either Standard or Extended addressing.
Select the Default button to return the settings to their default values.
- Select the Type tab.
- Select No Flow Control.
- Select the OK button to accept the connection configuration.
Released for: Schneider Electric India


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.