How can we help you today?

ISSymbol “Error connecting to server” on Web Thin Client and/or Secure Viewer: Error code 10061 (WSAECONNREFUSED) in EcoStruxure Machine SCADA Expert

Possible Reasons:
 TCP/IP Server is not running
 Port 1234 is blocked
 IP address is incorrect
 Network Security is blocking port

Solution:
Make sure IWS project is running
 Verify the TCP/IP Server task is started
 Verify the IP address in IIS matches the runtime device
 Allow port access in Firewall/Antivirus software
 Check Port availability using Telnet

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings