Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Getting Update Error Code 17 Could Not Update License during ClearScada License Update.
This error code, which happens to be the most common when using the dongle field exchange utility, is caused by extra blank space copied into the utility update field, usually from an email text page.

Possible Cause:
Additional blank spaces getting copied from an email, which are interpreted as additional characters by the utility, causing the allotted 265 character limit of each code to be exceeded and thus not recognized causing the error notice.

1

Possible Solution:

Double check the code to ensure by cross referencing the first and last digit from the email to the utility field. Click and place your cursor after the final digit and hit back space until the blank character fields between the cursor and final alphabetical character are removed. Click update license.

2

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings