Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the pinout details of BMXNOM0200 modbus port.

The table below shows the pin assignment for the serial port on the BMXNOM0200:

1


NOTE:
  • The two RS485 lines are isolated. The isolation voltage between the two serial lines 500 V and between each isolated serial line and the backplane is up to 500V AC.
  • The seven-wire RS232 and two-wire RS485 use the same female RJ45 connector. Only the signal cabling is different.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings