Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How over-voltage threshold works in ATV310

The ATV310 drive does not have a dedicated parameter to configure overvoltage protection. However, overvoltage conditions can be monitored using the fault relay status (R1 relay).

⚙️ Overvoltage Detection Range:

The drive monitors the line voltage from the perspective of the DC bus, whether the motor is running or stopped. This reflects the drive’s rated voltage. Typical voltage ranges include:

  • N4 model:
    • Input: 360V–460V, 3-phase
    • Output: 360V–460V, 3-phase

⚠️ When is Overvoltage Triggered?

  • At power-up: If the supply voltage exceeds 10% above the maximum acceptable level, an overvoltage condition may be detected.
  • When powered but not running: If the supply voltage exceeds 20% above the maximum rated line voltage, the drive may trigger an overvoltage fault.

Recommended Action:

Check the main supply voltage to ensure it remains within the acceptable range, especially during startup and idle conditions.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings