Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Customer has order the protection relay with the IEC60870-5-103 protocol instead of the Modbus protocol option. Do we have any add-on module for modbus that can be installed for this or any alternate solutions?
User needs to check the communication option at the time of ordering itself.
As per the selection of hardware, support of protocol is available.
Refer to the Cortec of the MICOM P54x & check the model number for the protocol support.
In case of hardware support is there, then the protocol option can be available by reflashing the relay with the correct firmware.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings