Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What to do if UPS SURT2000XLIM is not giving expected backup time?
Possible cause: Batteries are weak due to recent outage or are near end of service life.
Solution:  Charge the batteries. Batteries require recharging after extended outages. They wear faster when put into service often or when operated at elevated temperatures. If the battery pack is near the end of its service life, consider replacing it even if the Replace Battery LED is not yet lit.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings