Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to reduce motor noise in ATV610 drives.
For reduction in the motor noise, you may try to set the below parameters in the ATV610 drive:

1. Switch Frequency Type (SFt) - HF2

Allows the system to keep a constant chosen switching frequency [Switching frequency] SFr whatever the motor frequency [Output frequency] rFr. With this setting, the motor noise is kept as low as possible for a high switching frequency. In the event of overheating, the drive automatically decreases the switching frequency. It is restored to its original value when the temperature returns to normal.

2. Noise Reduction (nrd) - Yes

Random frequency modulation helps to prevent any resonance, which may occur at a fixed frequency.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings