Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does external fault feature means in LTMR/Tesys T
The LTM R controller has an external fault feature, which detects if an error happened on an external
system linked to it.

An external fault is triggered by setting a bit in the custom logic command register 1. This
external fault sets the controller into a fault state based on different parameters in the system.

An external fault can be reset only by clearing the external fault bit in the register.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings