Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What do if there is OL Error in the UPS model SRV2KL-IN?
Probable cause:

Easy-UPS is experiencing an overload condition

Possible Solution:

1.    Disconnect nonessential equipment from the Easy-UPS to eliminate the overload condition.
2.    Wait for the Easy-UPS to auto-recover.
3.    If still error is popped, restart the unit.
4.    Switch off the output, main power supply and then ON the utility power and ON the output.

In case if issue persist even after trying the above troubleshooting, log the complaint.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings